Inserting Images
When working in the Notes application on a desktop, use the Images option on the Insert menu to add an image to a Notes page.
Note: The option for inserting an image is not available when working on a handheld. However, you can transfer a file containing an image from your computer to a TI‑Nspire™ CX handheld and colors are retained. If transferred to a TI‑Nspire™ handheld, the colors in the image are converted to gray scale.
|
1.
|
Click from the Documents Toolbar. |
The Insert Image window opens.
|
2.
|
Navigate to the folder where the image is located. |
|
3.
|
Select the image, and then click to insert the image into the Notes work area. Valid files types are .jpg, .png, or .bmp. |
|
4.
|
To type text around the image, place the cursor in front of the image or after the image, and then type the text. |
Resizing an Image
Complete the following steps to resize an image.
|
1.
|
Click the image to select it. |
|
2.
|
Move the cursor to the edge of the image. |
The cursor changes to a left-right arrow symbol.
|
3.
|
Click the mouse and hold to enable the { tool, and then drag the image to make it smaller or larger. |
|
4.
|
Release the mouse button when the image is sized correctly. |
For more information, see Working with Images.