The TI Charging Station CE is shipped with the following components in each package:
| • | A TI Charging Station CE |
| • | An AC adapter |
| • | A regional power cord adapter |
| 1. | Insert the small end of the power adapter cord into the charging station’s power jack. |
| 2. | Plug the other end of the adapter into a power outlet. |
| • | An indentation on each side of the TI Charging Station CE enables you to lift it. Always use two hands to lift and move the charging station. |
| • | Place the charging station on a flat, stable surface. You can also use a wheeled cart if you need to move the charging station between classrooms. When deciding on a location, consider its proximity to a power source such as a power strip or wall outlet. |