Each simulation has features appropriate for the type of simulation. The table below is a quick guide to see the features and options in each simulation.
| • | The main menu will appear when you open the App. |
| • | Press ESC (press o) and YES (press o) to return to the main menu from a simulation. |
| • | To exit the application, select QUIT (press s) from the main menu. |
|
Menus |
Functions |
|---|---|
|
Main Menu |
|
|
Toss Coins |
Creates a simulation of a two-sided coin toss, and you have the option to weight the sides of the coin. You can flip up to 3 coins at once, and the number of heads is tallied. |
|
Roll Dice |
Creates a simulation of rolling up to three dice. The type of dice includes 6, 8, 10, 12, and 20 sides. The sum of the faces is tallied. |
|
Pick Marbles |
Creates a simulation of picking up to 5 different marbles from a bag. The simulation can run with or without replacement. The number of each type of marble in each pick is tallied. |
|
Spin Spinners |
Creates a simulation of one spinner with between 2 and 8 sections. Each section can be weighted. The spinner results are tallied. |
|
Draw Cards |
Creates a simulation of drawing one card at a time from a 52- or 32-card deck. For each pick, the number and suit are tallied. The draw of a card from the deck can be set with or without replacement from each draw. You can only use one deck at a time. |
|
Random Numbers |
Generates (draws) a set of up to 6 random numbers. The number range can be set from 0 to 99. Repetition or no repetition of numbers from the range can be set as an option. Each draw of the random set is tallied on the screen. |
|
OK |
Open the selected simulation. |
|
SEED |
Set the random seed value. |
|
ABOUT |
App version number information. |
|
QUIT |
Exit the application. |
|
Toss Coins |
|
|
ESC |
Return to the previous screen |
|
TOSS |
Toss one coin and access more tosses. |
|
SET (Settings) |
Change the settings for the simulation. |
|
Trial Set |
Tosses coin(s) as per trial settings and allows shortcut option to toss +1, +10, or +50 more tosses to add on to the simulation. Enter trial value from 1 to 999 tosses. |
|
Coins |
Set the number of coins tossed per trial to 1, 2, or 3. |
|
Graph |
Set graph display to frequency or simulated probability. Use right and left arrows on the bar graph view to display these values. |
|
StoTbl (Store Table) |
Set to No, All, or 50 to control the trials displayed in the table view. |
|
ClearTbl (Clear Table) |
Set to Yes if you want to clear the data of an existing simulation. |
|
Updates (Update After) |
Number of trials before the graph and data are updated. |
|
DATA |
Save the collected data to a list. |
|
TABLE |
Show a table of the trials. |
|
GRAPH |
Show a graph of the trials. |
|
Roll Dice |
|
|
ESC |
Return to the previous screen |
|
ROLL |
Rolls a die or dice as per trial settings and allows shortcut option to toss +1, +10, or +50 more rolls to add on to the simulation. |
|
SET (Settings) |
Change the settings for the simulation. |
|
Trial Set |
Enter trial value from 1 to 999. |
|
Dice |
Set the number of die or dice tossed per trial to 1, 2, or 3. |
|
Sides |
Set number of sides to 6, 8, 10, 12, or 20. |
|
Graph |
Set graph display to frequency or simulated probability. Use right and left arrows on the bar graph view to display these values. |
|
StoTbl (Store Table) |
Set to No, All, or 50 to control the trials displayed in the table view. |
|
ClearTbl (Clear Table) |
Set to Yes if you want to clear the data of an existing simulation. |
|
Updates (Update After) |
Number of trials before the graph and data are updated. |
|
DATA |
Save the collected data to a list. |
|
TABLE |
Show a table of the trials. |
|
GRAPH |
Show a graph of the trials. |
|
Pick Marbles |
|
|
ESC |
Return to the previous screen |
|
PICK |
Pick number of marbles as per trial settings. |
|
SET (Settings) |
Change the settings for the simulation. |
|
Trial Set |
Enter trial value from 1 to 999. |
|
Types |
Set the number of different types of marbles in the simulation to 1, 2, or 3. |
|
Graph |
Set graph display to frequency or simulated probability. Use right and left arrows on the bar graph view to display these values. |
|
StoTbl (Store Table) |
Set to No, All, or 50 to control the trials displayed in the table view. |
|
ClearTbl (Clear Table) |
Set to Yes if you want to clear the data of an existing simulation. |
|
Replace |
Yes: Replaces the marble after it is drawn. No: The marble is removed when it is drawn. |
|
Updates (Update After) |
Number of trials before the graph and data are updated. |
|
DATA |
Save the collected data to a calculator list. |
|
TABLE |
Show a table of the trials. |
|
GRAPH |
Show a graph of the trials. |
|
Spin Spinner |
|
|
ESC |
Return to the previous screen. |
|
SPIN |
Spins the spinner as per trial settings and allows shortcut option to toss +1, + 10, or +50 more spins to add on to the simulation. |
|
SET (Settings) |
Change the settings for the simulation. |
|
Trial Set |
Enter trial value from 1 to 999. |
|
Sections |
Set the number of sections of the spinner from 2 to 8 sections. |
|
Graph |
Set graph display to frequency or simulated probability. Use right and left arrows on the bar graph view to display these values. |
|
StoTbl (Store Table) |
Set to No, All, or 50 to control the trials displayed in the table view. |
|
ClearTbl (Clear Table) |
Set to Yes if you want to clear the data. |
|
Updates (Update After) |
Number of trials before the graph and data are updated. |
|
DATA |
Save the collected data to a list. |
|
TABLE |
Show a table of the trials. |
|
GRAPH |
Show a graph of the trials. |
|
Draw Cards |
|
|
ESC |
Return to the previous screen |
|
DRAW |
Draw one card. |
|
SET (Settings) |
Change the settings for the simulation. |
|
Decks |
Set to 1, 2, or 3 decks. |
|
Replace |
Yes: Replaces the card after it is drawn. No: The card is removed when it is drawn. |
|
Deck Size |
Set the card deck size to 52 or 32 cards. |
|
DATA |
Save the collected data to a list. |
|
CLEAR |
Clear all trials from memory. |
|
Random Number Sets |
|
|
ESC |
Return to the previous screen. |
|
Draw |
Roll one dice. |
|
SET (Settings) |
Change the settings for the simulation. |
|
Numbers |
Set between 1 and 6 random numbers per draw. |
|
Range |
Enter the range of numbers from 0 to 99. |
|
Repete |
Yes: Reuse numbers after they have been chosen. No: each trial will be unique. |
|
DATA |
Save the collected data to a list. |
|
CLEAR |
Clear all trials from memory. |
|
Advanced Options Menu |
|
|
ADV (Advanced) |
Set weight or probabilities for Toss Coin, Roll Dice, or Spin Spinner outcomes. Set the amount of each different marble in the simulation for Pick Marbles. |
See the graphing calculator’s Reference Guide for information on system error messages.
See the original app guidebook for more details on this application. Visit education.ti.com/go/download.