read()

Command:

read("obj","arg")

Command Syntax:

read("obj","arg")

Method:

read("obj","arg")

Object:

String that describes the TI-Innovator™ object that the READ command will be directed to.

Argument:

Contains a string with additional information needed for the READ operation such as index number of object, and other parameter values needed based on the value to read.

Range:

 

Describe:

Read a sensor value or other connected sensor or control value or property. Also can be used to read TI-Innovator™ specific information.

Result:

 

Error:

 

Type or
Addressable Component: