|
Command: |
|
|---|---|
|
Command |
|
|
Module: |
|
|
Describe: |
Clear the screen in the Shell environment. Row 0-11, integer may be used as an optional argument to clear a display row of the Shell environment. |
|
Python |
|
|
Result: |
Clear the screen in the Shell environment. Row 0-11, integer may be used as an optional argument to clear a display row of the Shell environment. |
|
Error: |
|
|
Type or |
from ti_system import* |
See Also: disp_clr()