This object is the interface to the brightness sensor on the TI-Innovator™ Hub.
It allows the program to read the value from the brightness sensor.
.
TI-Nspire CX II: from ti_hub import *
|
|
|
|
|
|
|
|
|
Command: |
TI-Nspire CX II: brightness.measurement() CE products: brightns.measurement() |
|---|---|
|
Command Syntax: |
brightness.measurement() |
|
Range: |
0 - 100 |
|
Describe: |
Returns the current internal reading from the on-board ambient light sensor. Example TI-Nspire CX II program:
|
|
Result: |
Read on-board light sensor level. |
|
Type or |
Control |
|
Command: |
TI-Nspire CX II: brightness.range() CE products: brightns.range() Advanced user |
|---|---|
|
Command Syntax: |
brightness.range([min, max]) |
|
Range: |
|
|
Describe: |
Changes/Sets the mapping of ADC input values from the ADC 0- 16383 range to a user-selected range. The resulting sensor reading is mapped to this and a floating point result is returned. By default, the on-board BRIGHTNESS sensor is ranged to a 0-100 range. |
|
Result: |
Set mapping for on-board brightness/light sensor. |
|
Type or |
Sensor |