TI-Nspire™ Python includes the following modules:
|
Standard Modules |
TI Modules |
|---|---|
|
Math (math) Random (random) Complex Math (cmath) Time (time) |
TI PlotLib (ti_plotlib) TI Hub (ti_hub) TI Rover (ti_rover) TI System (ti_system) TI Draw (ti_draw) TI Image (ti_image) |
Note: If you have existing Python programs created in other Python development environments, you may need to edit them to run on the TI-Nspire™ Python solution. Modules may use different methods, arguments, and ordering of methods in a program compared to the TI modules. In general, be aware of compatibility when using any version of Python and Python modules.
When transferring Python programs from a non-TI platform to a TI platform OR from one TI product to another, remember:
| • | Programs that use core language features and standard libs (math, random, etc.) can be ported without changes. |
| • | Programs that use platform-specific libraries such as matplotlib for PC or TI modules will require edits before they will run on a different platform. This may be true even between TI platforms. |
As with any version of Python, you will need to include imports to use any functions, methods, or constants contained in a given module. For example, to execute the cos() function from the math module, use the following commands:
>>>from math import *
>>>cos(0)
1.0
For a list of menus with their items and descriptions, please see the Menu Map section.