You can find probability features in the » PROB submenu.
Many probability features have Stat Wizards to help you enter the syntax.
Example:
To generate a set of five random integers between 10 and 25 (inclusive):
1. | Press », then press ~ until you highlight PROB. |
2. | Press † until you highlight 5: randInt(, then [enter]. |
3. | Enter the lower integer, then [enter]. |
4. | Enter the upper integer, then [enter]. |
5. | Enter the number of integers (n), then [enter]. |
6. | Press [enter] to Paste. |
7. | Press [enter] again to see the random set of integers. |
Note:
• | With each rand execution, the TI-84 Plus CE App for Chrome OS™ generates the same random-number sequence for a given seed value. The TI-84 Plus CE App for Chrome OS™ factory-set seed value for rand is 0. To generate a different random-number sequence, store any nonzero seed value to rand. To restore the factory-set seed value, store 0 to rand, or reset the defaults by going to y L 7:Reset... 2:Defaults.... |
• | The seed value also affects randInt(, randNorm(, and randBin( instructions. |