Using Color on the TI-84 Plus CE App for Chrome OS™
The TI-84 Plus CE App for Chrome OS™ has many color options and a high resolution display that allows more information to be shown on the screen. The TI-84 Plus CE App for Chrome OS™ uses color in the following ways:
|
•
|
Y= editor for line color. |
|
•
|
DRAW commands for line color, such as vertical lines, circles, and text on the graph screen. |
|
•
|
The graph format screen for grid, axes, or border color, and applying a background image or color. |
Color options for various features are accessed via a spinner menu. With the cursor on a color selection for a feature, use the | or ~ to change the color. When the cursor is on any spinner menu, the context help in the status bar frequently displays the hint: PRESS [<] OR [>] TO SELECT AN OPTION.
Note: Take care to choose appropriate color combinations for the graph areas so that all features are visible.
Resetting Color Options to Default
|
•
|
With the cursor on a function in [Y=], press ‘ ‘ to return to the default color and line style for that function. |
|
•
|
You can reset the calculator to its default settings, including color settings, by pressing y L |
Topic Links