Features in the TI-84 Plus CE App for Chrome OS™

• CE OS v 5.4 math features!
• Familiar 5 Pre-loaded Image Vars for modeling

• When App is launched, the emulator always returns to the default state (as shown here.)
– Tip: [2nd] [quit] to the Home Screen from RAM Cleared screen.

 

Emulator Window Sizing

The emulator window snaps to size as any window on Chrome OS™.

• Resize the emulator window as needed to “stage” your windows.
• Tip: See 84 Activity Central for activities to support for your remote teaching.
- See https://education.ti.com/en/84activitycentral/us/home

 

Pressing Emulator Keys in Chrome OS™

• Touch Screen - Touch each emulator key
• Mouse - click away on the emulator keys!
– Tip: Check Mouse speed and acceleration settings
– Settings > Device > Mouse and touchpad
– Tip: Highlight mouse cursor when it is moving?
– Settings > Device > Accessibility > Manage Accessibility Features

• Touchpad – touch the emulator keys!
– Tip: Check Touchpad speed and acceleration
– Settings > Device > Mouse and touchpad
• SmartPad CE App on a connected TI-84 Plus CE:
– Teacher tip: If you have your TI-84 Plus CE and the USB computer cable, connect and use the SmartPad CE App.
– For Students: SmartPad CE App is preloaded if they have the TI-84 Plus CE at home. However, be aware they may not have the USB computer cable at hand.