var.recallAt(name, col [,row])
Recalls a value from a cell of a list or matrix in the symbol table. col is a 1-based column number of the matrix or list. row is a 1-based row number. row is only required when recalling a value from a matrix.
This function is optimized to work with numeric values and normally
returns a number. If the value of the recalled cell is not numeric, this
function returns nil and an error message
string.
Introduced in platform.apiLevel = '2.0'