var.makeNumericList(name)
Creates a list in the symbol table with the given name. The list is optimized to hold numeric values. Routines storeAt and recallAt operate much more efficiently on lists that are created with this function.
Usage Note
This function cannot be used to create a numeric matrix. Routines
var.recallAt and var.storeAt documented below will work with matrices but only
if they are created by some other means (see Listing
18.1).
Listing 18.1: Example for Accessing a Matrix via the Variable Library
var.store("mat", {{1,2}, {3,4}}) -- creates matrix mat
var.storeAt("mat", 13.3, 1, 1)
val = var.recallAt("mat", 1, 1)
Introduced in platform.apiLevel = '2.0'