You are here: Lua Scripting Resources eGuide > Lua Scripting API Reference Guide > Timer Library > start

16.2 start

timer.start(period)

Starts the timer with the given period in seconds. The period must be ≥ 0.01 (10 ms). If the timer is already running when this routine is called, the timer is reset to the new period.

Introduced in platform.apiLevel = '1.0'

Caution

timer.start() should not be called when processing an on.timer() event unless it is the final statement before the on.timer() event completes.