self = physics.Space:resizeStaticHash(dim, count)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Space |
The input simulation Space |
|
dim |
in number |
The length of one side of a hash cell. Default is 100 count |
|
count |
in number |
The number of cells in the hash table. Default is 1000 |
|
self |
out physics.Space |
The input Space is returned as the output |
This routine configures the spatial hash of static Shapes. Configure this similarly to resizeActiveHash but for static Shapes.
.Introduced in platform.apiLevel = '2.0'