self = physics.Shape:setSurfaceV(vel)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Shape |
The input Shape |
|
velgroup |
in physics.Vect |
The new vector for the surface velocity |
|
self |
out physics.Shape |
The input Shape is returned as the output |
Sets the surface velocity of the shape. Returns self.
Note
The group number is converted to a positive whole number when stored.
Introduced in platform.apiLevel = '2.0'