self = physics.Shape:setRestitution(r)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Shape |
The input Shape |
|
r |
in number |
The new value for the shape’s restitution |
|
self |
out physics.Shape |
The input Shape is returned as the output |
Sets the restitution (or elasticity) of the shape. A value of 0.0 gives no bounce and a value of 1.0 gives a perfect bounce. Returns self.
Note
May not behave as expected for r larger than 1.0 or less than 0.
Introduced in platform.apiLevel = '2.0'