self = physics.Shape:setLayers(layers)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Shape |
The input Shape |
|
layers |
in number |
A bitmap of integer layer numbers. This implementation permits 32 layers |
|
self |
out physics.Shape |
The input Shape is returned as the output |
Sets the layers that the shape inhabits. Shapes only collide if they are in the same layer. layers is an integer bitmap of all the layers that the shape occupies. Returns self.
Introduced in platform.apiLevel = '2.0'