info = physics.Shape:segmentQuery(vecta, vectb)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Shape |
The input Shape |
|
vecta |
in physics.Vect |
One end point of the segment |
|
vectb |
in physics.Vect |
The other end point of the segment |
|
info |
out physics.SegmentQueryInfo |
Information about where the segment and Shape intersect. Nil if no intersection |
Checks if the line
segment from vecta to vectb intersects the Shape.
Returns a
SegmentQueryInfo object with the result of the query or nil if no
intersection.
If a segment query starts inside of a shape then the result is somewhat undefined. Circles and polygons will not report a collision with that shape, and segments will report an incorrect point and normal if they do detect a collision with that shape. To get around this deficiency, use a separate point query to determine if the segment query starts inside of a shape.
See the SegmentQueryInfo methods below for helper routines to convert the results to world coordinates or absolute distance.
Introduced in platform.apiLevel = '2.0'