self = physics.Body:setWLimit(limit)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Body |
The input Body |
|
limit |
in number |
The maximum angular velocity of the Body |
|
self |
out physics.Body |
The input Body is returned as the output |
Updates the limit of the angular velocity of the body. Angular velocity is in radians per unit time.
Returns the Body.
Introduced in platform.apiLevel = '2.0'