self = physics.Body:setAngVel(vel)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Body |
The input Body |
|
vel |
in number |
The angular velocity in radians per unit time of the Body |
|
avel |
out number |
The input Body is returned as the output |
Updates the angular velocity of the body. The angular velocity is in radians per unit time.
Returns the Body.
Introduced in platform.apiLevel = '2.0'