self = physics.Arbiter:setFriction(friction)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Arbiter |
The input Arbiter |
|
f |
in number |
Friction in the collision |
|
self |
out physics.Arbiter |
The input Arbiter is returned as the output |
Overrides the calculated friction of the collision.
Note
May not behave as expected for f larger than 1.0 or less than 0.
Introduced in platform.apiLevel = '2.0'