error = bleCentral.startScanning([UUID, ] callback [, object])
Scans for Bluetooth® LE devices advertising a service with the given service UUID (Universal Unique Identifier) or for Bluetooth® LE devices advertising any service if no UUID is provided. Successive calls of startScanning automatically stop previous scans. A malformed UUID will cause a Lua error as this is an authoring error and not a run-time error..
|
Parameter |
Type |
Description |
|---|---|---|
|
UUID |
in string |
UUID of the service searched
for. |
|
callback |
in function |
Callback to receive asynchronously
peripherals |
|
object |
in any |
If an object is provided it will be passed as the
first parameter to the specified callback function. |
|
error |
out string |
If successful nil is returned, an error message otherwise |
Introduced in platform.apiLevel = '2.5'
callback([object,] peripheral, advertisementData, isConnectable, RSSI)
The callback function provided in startScanning will be called for every Bluetooth® LE device fulfilling the search criteria. The peripheral parameter will be a peripheral object representing the found Bluetooth® LE device. The same peripheral object might be reported more than once based on peripheral and platform behavior.
|
Parameter |
Type |
Description |
|---|---|---|
|
object |
in any |
If an object was provided as a parameter to the function startScanning, it will be passed as the first parameter to this callback function |
|
peripheral |
in peripheral object |
One peripheral found during scanning |
|
advertisementData |
in table |
A table containing the
advertisement data of the |
|
isConnectable |
in boolean |
true if the device advertises as connectable, otherwise false |
|
RSSI |
in Integer value |
The received signal strength indicator (RSSI) in dbm. |
The constants described in the following table are part of the ble table, e.g.
ble.AD TX POWER LEVEL.
|
Name |
Description |
|---|---|
|
AD NAME |
Same as the device name or a shortened name. Please see subsection 20.3.1 for peripheral:getName(). |
|
AD MANUFACTURER DATA |
Bluetooth® technology is switched off. This implies that any A string with the first 2 octets identifying the manufacturer (see Company Identifiers.). The interpretation of any other octet in the string is manufacturer specific. |
|
AD SERVICE UUIDS |
A list of service UUIDs. This list might be complete or not. |
|
AD TX POWER LEVEL |
If provided by the device, the sending power level of the device in dBm. Subtracting the RSSI value from the power level can be used to compare the approximate distance of different devices |
Introduced in platform.apiLevel = '2.5'
Extended in platform.apiLevel = ‘2.6'