You are here:TI‑Nspire™/TI‑Nspire™ CX Reference Guide > X

X

xor

BooleanExpr1 xor BooleanExpr2 returns Boolean expressionBooleanList1
xor BooleanList2 returns Boolean listBooleanMatrix1
xor BooleanMatrix2 returns Boolean matrix

Returns true if BooleanExpr1 is true and BooleanExpr2 is false, or vice versa.

Returns false if both arguments are true or if both are false. Returns a simplified Boolean expression if either of the arguments cannot be resolved to true or false.

Note: See or, here.

Integer1 xor Integer2 integer

Compares two real integers bit-by-bit using an xor operation. Internally, both integers are converted to signed, 64-bit binary numbers. When corresponding bits are compared, the result is 1 if either bit (but not both) is 1; the result is 0 if both bits are 0 or both bits are 1. The returned value represents the bit results, and is displayed according to the Base mode.

You can enter the integers in any number base. For a binary or hexadecimal entry, you must use the 0b or 0h prefix, respectively. Without a prefix, integers are treated as decimal (base 10).

If you enter a decimal integer that is too large for a signed, 64-bit binary form, a symmetric modulo operation is used to bring the value into the appropriate range. For more information, see Base2,  here.

Note: See or, here.

In Hex base mode:

Important: Zero, not the letter O.


In Bin base mode:

Note: A binary entry can have up to 64 digits (not counting the 0b prefix). A hexadecimal entry can have up to 16 digits.