You are here:TI‑Nspire™ CAS/TI‑Nspire™ CX CAS Reference Guide > Warning Codes and Messages

Warning Codes and Messages

You can use the warnCodes() function to store the codes of warnings generated by evaluating an expression. This table lists each numeric warning code and its associated message. For an example of storing warning codes, see warnCodes(), here.

Warning code


Message

10000

Operation might introduce false solutions.

10001

Differentiating an equation may produce a false equation.

10002

Questionable solution

10003

Questionable accuracy

10004

Operation might lose solutions.

10005

cSolve might specify more zeros.

10006

Solve may specify more zeros.

10007

More solutions may exist. Try specifying appropriate lower and upper bounds and/or a guess.

Examples using solve():

solve(Equation, Var=Guess)|lowBound<Var<upBound
solve(Equation, Var)|lowBound<Var<upBound
solve(Equation, Var=Guess)

10008

Domain of the result might be smaller than the domain of the input.

10009

Domain of the result might be larger than the domain of the input.

10012

Non-real calculation

10013

^0 or undef^0 replaced by 1

10014

undef^0 replaced by 1

10015

1^ or 1^undef replaced by 1

10016

1^undef replaced by 1

10017

Overflow replaced by or

10018

Operation requires and returns 64 bit value.

10019

Resource exhaustion, simplification might be incomplete.

10020

Trig function argument too big for accurate reduction.

10021

Input contains an undefined parameter.

Result might not be valid for all possible parameter values.

10022

Specifying appropriate lower and upper bounds might produce a solution.

10023

Scalar has been multiplied by the identity matrix.

10024

Result obtained using approximate arithmetic.

10025

Equivalence cannot be verified in EXACT mode.

10026

Constraint might be ignored. Specify constraint in the form "\" 'Variable MathTestSymbol Constant' or a conjunct of these forms, for example 'x<3 and x>-12'