Catalog > |
||||||||||
bal(NPmt,N,I,PV ,[Pmt], [FV], [PpY], [CpY], [PmtAt], [roundValue]) ⇒ value bal(NPmt,amortTable) ⇒ value Amortization function that calculates schedule balance after a specified payment. N, I, PV, Pmt, FV, PpY, CpY, and PmtAt are described in the table of TVM arguments, here. NPmt specifies the payment number after which you want the data calculated. N, I, PV, Pmt, FV, PpY, CpY, and PmtAt are described in the table of TVM arguments, here.
roundValue specifies the number of decimal places for rounding. Default=2. bal(NPmt,amortTable) calculates the balance after payment number NPmt, based on amortization table amortTable. The amortTable argument must be a matrix in the form described under amortTbl(), here. Note: See also ΣInt() and ΣPrn(), here. |
|
Catalog > |
|
Integer1 ►Base2 ⇒ integer Note: You can insert this operator from the computer keyboard by typing @>Base2. Converts Integer1 to a binary number. Binary or hexadecimal numbers always have a 0b or 0h prefix, respectively. Use a zero, not the letter O, followed by b or h. 0b binaryNumber |
|
A binary number can have up to 64 digits. A hexadecimal number can have up to 16. Without a prefix, Integer1 is treated as decimal (base 10). The result is displayed in binary, regardless of the Base mode. Negative numbers are displayed in “two's complement” form. For example, ⁻1 is displayed as ⁻263 is displayed as If you enter a decimal integer that is outside the range of a signed, 64-bit binary form, a symmetric modulo operation is used to bring the value into the appropriate range. Consider the following examples of values outside the range. 263 becomes ⁻263 and is displayed as 264 becomes 0 and is displayed as ⁻263 − 1 becomes 263 − 1 and is displayed as |
|
Catalog > |
|
Integer1 ►Base10 ⇒ integer Note: You can insert this operator from the computer keyboard by typing @>Base10. Converts Integer1 to a decimal (base 10) number. A binary or hexadecimal entry must always have a 0b or 0h prefix, respectively. 0b binaryNumber Zero, not the letter O, followed by b or h. A binary number can have up to 64 digits. A hexadecimal number can have up to 16. Without a prefix, Integer1 is treated as decimal. The result is displayed in decimal, regardless of the Base mode. |
|
Catalog > |
|
Integer1 ►Base16 ⇒ integer Note: You can insert this operator from the computer keyboard by typing @>Base16. Converts Integer1 to a hexadecimal number. Binary or hexadecimal numbers always have a 0b or 0h prefix, respectively. 0b binaryNumber Zero, not the letter O, followed by b or h. A binary number can have up to 64 digits. A hexadecimal number can have up to 16. Without a prefix, Integer1 is treated as decimal (base 10). The result is displayed in hexadecimal, regardless of the Base mode. If you enter a decimal integer that is too large for a signed, 64-bit binary form, a symmetric modulo operation is used to bring the value into the appropriate range. For more information, see ►Base2, here. |
|
Catalog > |
|
binomCdf(n,p) ⇒ list binomCdf(n,p,lowBound,upBound) ⇒ number if lowBound and upBound are numbers, list if lowBound and upBound are lists binomCdf(n,p,upBound)for P(0≤X≤upBound) ⇒ number if upBound is a number, list if upBound is a list Computes a cumulative probability for the discrete binomial distribution with n number of trials and probability p of success on each trial. For P(X ≤ upBound), set lowBound=0 |
|
Catalog > |
|
binomPdf(n,p) ⇒ list binomPdf(n,p,XVal) ⇒ number if XVal is a number, list if XVal is a list Computes a probability for the discrete binomial distribution with n number of trials and probability p of success on each trial. |
|