You can use the
Warning code |
|
|||||||||
10000 |
Operation might introduce false solutions. |
|||||||||
10001 |
Differentiating an equation may produce a false equation. |
|||||||||
10002 |
Questionable solution |
|||||||||
10003 |
Questionable accuracy |
|||||||||
10004 |
Operation might lose solutions. |
|||||||||
10005 |
cSolve might specify more zeros. |
|||||||||
10006 |
Solve may specify more zeros. |
|||||||||
10007 |
More solutions may exist. Try specifying appropriate lower and upper bounds and/or a guess. Examples using solve():
|
|||||||||
10008 |
Domain of the result might be smaller than the domain of the input. |
|||||||||
10009 |
Domain of the result might be larger than the domain of the input. |
|||||||||
10012 |
Non-real calculation |
|||||||||
10013 |
∞^0 or undef^0 replaced by 1 |
|||||||||
10014 |
undef^0 replaced by 1 |
|||||||||
10015 |
1^∞ or 1^undef replaced by 1 |
|||||||||
10016 |
1^undef replaced by 1 |
|||||||||
10017 |
Overflow replaced by ∞ or −∞ |
|||||||||
10018 |
Operation requires and returns 64 bit value. |
|||||||||
10019 |
Resource exhaustion, simplification might be incomplete. |
|||||||||
10020 |
Trig function argument too big for accurate reduction. |
|||||||||
10021 |
Input contains an undefined parameter. Result might not be valid for all possible parameter values. |
|||||||||
10022 |
Specifying appropriate lower and upper bounds might produce a solution. |
|||||||||
10023 |
Scalar has been multiplied by the identity matrix. |
|||||||||
10024 |
Result obtained using approximate arithmetic. |
|||||||||
10025 |
Equivalence cannot be verified in EXACT mode. |
|||||||||
10026 |
Constraint might be ignored. Specify constraint in the form "\" 'Variable MathTestSymbol Constant' or a conjunct of these forms, for example 'x<3 and x>-12' |