Error Condition |
New message |
---|---|
Error in condition statement (If/While) |
A conditional statement did not resolve to TRUE or FALSE NOTE: With the change to place the cursor on the line with the error, we no longer need to specify if the error is in an "If" statement or a "While" statement. |
Missing EndIf |
Expected EndIf but found a different end statement |
Missing EndFor |
Expected EndFor but found a different end statement |
Missing EndWhile |
Expected EndWhile but found a different end statement |
Missing EndLoop |
Expected EndLoop but found a different end statement |
Missing EndTry |
Expected EndTry but found a different end statement |
“Then” omitted after If <condition> |
Missing If..Then |
“Then” omitted after ElseIf <condition> |
Then missing in block: ElseIf. |
When “Then”, “Else” and “ElseIf” were encountered outside of control blocks |
Else invalid outside of blocks: If..Then..EndIf or Try..EndTry |
“ElseIf” appears outside of “If..Then..EndIf” block |
ElseIf invalid outside of block: If..Then..EndIf |
"Then” appears outside of “If....EndIf” block |
Then invalid outside of block: If..EndIf |
In case commands that expect one or more arguments are called with an incomplete list of arguments, a “Too few argument error” will be issued instead of “syntax” error
Current behavior |
New CX II behavior |
---|---|
|
|
|
|
|
|
|
|
Note: When an incomplete list of arguments is not followed by a comma, the error message is: “too few arguments”. This is the same as previous releases.