Creating Shapes Using Gestures (MathDraw)
The MathDraw tool lets you use touchscreen or mouse gestures to create points, lines, circles and other shapes.
MathDraw is available in:
• | Geometry view without the analytic window displayed. |
• | Graphing view when the x scale and y scale are identical. This avoids non-circular ellipses and non-square rectangles appearing as circles and squares. |
MathDraw is not available in the 3D Graphing view or in the Geometry view with the analytic window displayed.
Activating MathDraw
1. | If using the Geometry view with the analytic window visible, use the View menu to hide the window. |
2. | On the Actions menu, select MathDraw. |
The MathDraw icon appears. You can begin using the tool.
Cancelling MathDraw
▶ | When you have finished using the MathDraw tool, press Esc. |
The tool also closes if you select a different tool or change views.