Graphing a Family of Functions
In a family of functions, each member has its own value for one or more of the parameters. By entering the parameters as lists, you can use a single expression to graph a family of up to 16 functions.
For example, the expression
f1_1(x) = -1 • x + 2
f1_2(x) = 0 • x + 4
f1_3(x) = 1 • x + 6
f1_4(x) = 2 • x + 8
To Graph a Family of Functions
| 1. | From the Graph Entry/Edit menu, select Function. |
| 2. | Type the expression, using lists to represent the members of the family. |
| 3. | Press Enter to graph the functions. |
Each member is labelled separately (f1_1, f1_2, and so on) to indicate its sequence in the expression.
Note: You cannot edit a single function graph to change it to a family of functions.