Inserting Comments, Shapes and Calculations
You can insert Teacher or Review comments into a Notes page. Comments are labeled to make them easy to distinguish from the original text.
1. | Tap the Notes work area where you want to insert a comment. |
2. | Tap Tools ![]() |
3. | Tap Comment. |
4. | Tap Teacher or Reviewer to choose the comment type. |
5. | Type the comment text inside the comment box. |
The comment text appears in bold formatting.
6. | If needed, select the text and tap Inspector ![]() |
Use geometric shapes to designate selected text as a geometric object such as an angle, circle or line segment.
1. | Tap the work area where you want to insert the shape, or select the text that you want designate as a shape. |
2. | Tap Tools ![]() |
3. | Tap Shape. |
4. | Tap the shape name (such as segment or ray) to insert it before the selected item. |
1. | Tap the Notes work area to place your cursor where you want to insert the maths expression. |
2. | Tap Tools ![]() |
3. | Tap the type of calculation you want to insert, and then tap the function name to insert the expression. |