Using Wireless Communication Hardware

Teachers using TI-Nspire™ CX Premium Teacher Software in the classroom can attach wireless cradles and/or network adapters to students' TI-Nspire™ CX handhelds. Those handhelds can then link wirelessly to an access point attached to the teacher's computer.

You can attach any the following devices to TI-Nspire™ CX handhelds:

• TI-Nspire™ CX Wireless Network Adapter - v2 (2.4 GHz or 5.0 GHz band)
• TI-Nspire™ Wireless Network Adapter (2.4 GHz)

Attaching a Wireless Adapter to a CX Handheld

Note: The battery in the handheld powers the wireless adapter.

1. Position the wireless adapter on top of the handheld so the connector on the adapter lines up with the connector on top of the handheld.

 

Wireless network adapter (school-owned)

 

 

 

Connector

Guides for aligning with handheld

2. Slide the adapter into position, making sure the guides on the sides of the adapter slide into the grooves on the sides of the handheld.

 

Side view of handheld

Groove to align wireless adapter

3. Firmly press the adapter into place so that the adapter sits on top of the handheld as shown in the following illustration.

Note: The TI-Nspire™ CX handheld can be charged with the wireless adapter attached.