Using Settings and Status

When working with the TI-SmartView™ emulator, you can change General Settings and Document Settings. For more information, see Using the Documents Workspace.

You can view all other settings, but you cannot change them in the TI-SmartView™ emulator. However, the ability to view these options provides teachers with an instructional tool when they need to show students how to set up a handheld.

To view settings and status:

1. Click c to access the Home screen.
2. Click Settings.

 

Setting or Settings

Description

Language

You can open the languages menu and select a language, but you cannot save changes. To change the language, use the TI-Nspire™ menu File > Settings > Change Language option.

Handheld Setup

You can open the menus and select items to demonstrate which items to choose, but you cannot save any changes.

Handheld Status

You can access the screen. The # symbol replaces any numeric values that would be displayed on the handheld.

About

You can open the About screen and view the software version. Other information that pertains only to the handheld hardware is marked as "Not Applicable."

Login

You can display the Login to Class screen and type in the User Name and Password fields. Login is not available.