Inserting Items from the Catalog
You can use the Catalog to insert functions and commands, symbols, and expression templates into the entry line.
1. | Press k to open the Catalog. By default, the first tab is displayed, which lists all commands and functions in alphabetical order. |
2. | If the function you are inserting is visible in the list, select it and press · to insert it. |
3. | If the function is not visible: |
a) | Press a letter key to jump to the entries that begin with that letter. |
b) | Press ¤ or £ as necessary to highlight the item you are inserting. |
c) | Click a numbered tab to list functions by category: math functions, symbols, math templates, library objects, and value for standard measurement units. |
d) | Press · to insert the item into the entry line. |
Using an Expression Template
Templates help you enter matrices, piecewise functions, systems of equations, integrals, derivatives, products, and other math expressions.
For example, suppose you want to evaluate
1. | Press t to open the Template palette. |
2. | Select ![]() |
The template appears on the entry line with small blocks representing elements that you can enter. A cursor appears next to one of the elements to show that you can type a value for that element.
3. | Use the arrow keys to move the cursor to each element’s position, and type a value or expression for each element. |
4. | Press · to evaluate the expression. |
Inserting Expressions Using a Wizard
You can use a wizard to simplify entering some expressions. The wizard contains labeled boxes to help you enter the arguments in the expression.
For example, suppose you want to fit a y=mx+b linear regression model to the following two lists:
{1,2,3,4,5}
{5,8,11,14,17}
1. | Press k 1 to open the Catalog and show the alphabetic list of functions. |
2. | Click inside the list, and then press L to jump to the entries that begin with “L.” |
3. | Press ¤ as necessary to highlight LinRegMx. |
4. | If the Wizards On option is not checked, press e e to highlight Wizards On. |
5. | Press · to change the setting. |
6. | Press e e to highlight LinRegMx again. |
|
|
LinRegMx function in a non-CAS or Exact Arithmetic handheld |
|
|
LinRegMx function in a CAS handheld |
7. | Press ·. |
A wizard opens, giving you a labeled box to type each argument.
8. | Type {1,2,3,4,5} as X List. |
9. | Press e to move to the Y List field. |
10. | Type {5,8,11,14,17} as Y List. |
11. | If you want to store the regression equation in a specific variable, press e, and then replace Save RegEqn To with the name of the function variable (f1 through f99). |
12. | Click OK to close the wizard and insert the expression into the entry line. |
The expression is inserted along with statements to copy the regression equation and display the variable stat.results, which will contain the results.
LinRegMx {1,2,3,4,5},{5,8,11,14,17},1: CopyVar stat.RegEqn,f1: stat.results
The Scratchpad then displays the stat.results variables.
Note: You can copy values from the stat.results variables and paste them into the entry line.