Calculating with Scratchpad
From the Scratchpad Calculate page, enter a math expression on the entry line, and then press · to evaluate the expression. Expressions are displayed in standard mathematical notation as you enter them.
Each evaluated expression and result becomes part of the Scratchpad history, displayed above the entry line.
Entering Simple Math Expressions
Note: To enter a negative number, press v and then type the number.
1. | Select the entry line in the work area. |
2. | Type 2 l 8 to begin the expression. |
3. | Press ¢ to return the cursor to the baseline, and then complete the expression by typing: r 43 p 12 |
4. | Press · to evaluate the expression. |
The expression is displayed in standard mathematical notation, and the result is displayed on the right side of the page.
Note: You can force a decimal approximation in a result by pressing / · instead of ·.
|
Note: Results formatting can also be adjusted in settings. For more information about customizing settings, see Configuring Handhelds.