Changing the Aspect Ratio
The Review Workspace displays graphs in a question application as they appear on the students’ handhelds or computers. At times, the graphs may appear stretched, since the graph may have changed the aspect ratio to fit on the handheld.
You can select to view the graphs as they come in from students, or you can preserve the aspect ratio of the graph as it appeared when it was inserted in the question application.
By default, the Review Workspace displays graphs in a question application as they appear when the students submit them.
To preserve the aspect ratio of a graph as it appeared when it was inserted in the question, follow these steps:
1. | View the data in graph view. |
2. | Right-click on the graph in the Data View pane, and then click Graph Tools > Aspect Ratio. |
— or —
3. | Click ![]() |
When the Aspect Ratio box is checked, the aspect ratio is preserved. When the box is not checked, the aspect ratio may change.