USA FCC Information Concerning Radio Frequency Interference
|
Product Name |
FCC ID |
|
TI-Nspire™ Navigator™ Wireless Cradle |
V7R-TINAVWC2 |
|
TI-Nspire™ Navigator™ Access Point |
V7R-TINAVAP2 |
|
TI-Nspire™ CX Wireless Network Adapter |
V7R-TINAVWNA |
|
TI-Nspire™ CX Navigator™ Access Point |
V7R-TINAVAP3 |
|
TI-Nspire™ CX Navigator™ Wireless Network Adapter – v2 |
V7R-TINAVWNA2 |
FCC Compliance Statement
This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to Part 15 of the FCC Rules.
Operation is subject to the following two conditions: (1) These devices may not cause harmful interference, and (2) these devices must accept any interference received, including interference that may cause undesired operation.
The device for the band 5150-5250 MHz is only for indoor usage to reduce potential for harmful interference to co-channel mobile satellite systems.
RF Radiation Exposure and Hazard Statement
To ensure compliance with Federal Communications Commission (USA) requirements, (SAR limit is 1.6 W/kg averaged over one gram of tissue), the products listed in the following table have been evaluated under FCC Bulletin OET 65C and found to be compliant with the requirements in 47 CFR Part 2.1093 for RF exposure from radio frequency devices.
The highest SAR value reported under this standard during product certification when worn on the body:
|
Product Name |
SAR Value |
|
TI-Nspire™ Navigator™ Wireless Cradle |
0.562 W/kg |
|
TI-Nspire™ Navigator™ Access Point |
0.995 W/kg |
|
TI-Nspire™ CX Wireless Network Adapter |
0.994 W/kg |
|
TI-Nspire™ CX Navigator™ Access Point |
0.433 W/Kg |
|
TI-Nspire™ CX Navigator™ Wireless Network Adapter – v2 |
0.716 W/Kg |
Using higher gain antennas and types of antennas not covered under the FCC certification of this product is not allowed. Installers of the radio and end users of the product must adhere to the installation instructions provided in this manual.
This transmitter must not be co-located or operating in conjunction with any other antenna or transmitter.
Non-modification Statement
Use only the integral antenna supplied by the manufacturer when operating these devices. Unauthorized antennas, modifications, or attachments could damage the TI-Nspire™ Navigator™ Cradle, TI-Nspire™ Navigator™ Access Point, TI-Nspire™ CX Wireless Network Adapter, TI-Nspire™ CX Navigator™ Access Point, or TI-Nspire™ CX Navigator™ Network Adapter – v2 and violate FCC regulations. Any changes or modifications not expressly approved by the party responsible for compliance could void the user's authority to operate this equipment.