Canadian IC Information
Product Name |
IC |
TI-Nspire™ Navigator™ Wireless Cradle |
451E-TINAVWC2 |
TI-Nspire™ Navigator™ Access Point |
451F-TINAVAP2 |
TI-Nspire™ CX Wireless Network Adapter |
451E-TINAVWNA |
TI-Nspire™ CX Navigator™ Access Point |
451F-TINAVAP3 |
TI-Nspire™ CX Navigator™ Wireless Network Adapter – v2 |
451F-TINAVWNA2 |
Industry Canada Statement
This device complies with Industry Canada license-exempt RSS standard(s). Operation is subject to the following two conditions:
1. | This device may not cause interference, and |
2. | This device must accept any interference, including interference that may cause undesired operation of the device. |
To ensure compliance with Industry Canada requirements, (SAR limit is 1.6 W/kg averaged over one gram of tissue), these products have been evaluated and found compliant in accordance with Industry Canada RSS-102 with respect to the Safety Code 6 for Human Exposure to RF Fields.
The highest SAR value reported under this standard during product certification when worn on the body:
Product Name |
SAR Value |
TI-Nspire™ Navigator™ Wireless Cradle |
0.562 W/kg |
TI-Nspire™ Navigator™ Access Point |
0.995 W/kg |
TI-Nspire™ CX Wireless Network Adapter |
0.994 W/kg |
TI-Nspire™ CX Navigator™ Access Point |
0.433 W/Kg |
TI-Nspire™ CX Navigator™ Wireless Network Adapter – v2 |
0.716 W/Kg |
Equipment (or its transmit antenna) that is installed outdoors is subject to licensing and not supported by the listed products.
More information may be found in RSS-102 (http://www.ic.gc.ca/eic/site/smt-gst.nsf/eng/sf01904.html) and in Canada’s Safety Code 6 (http://www.hc-sc.gc.ca/ewh-semt/pubs/radiation/radio_guide-lignes_direct-eng.php).
Under Industry Canada regulations, this radio transmitter may only operate using an antenna of a type and maximum (or lesser) gain approved for the transmitter by Industry Canada. To reduce potential radio interference to other users, the antenna type and its gain should be so chosen that the equivalent isotropically radiated power (e.i.r.p.) is not more than that necessary for successful communication.
The device for the band 5150-5250 MHz is only for indoor usage to reduce potential for harmful interference to co-channel mobile satellite systems.
CAN ICES-3(B)/NMB-3(B)
Industrie Canada Déclaration
Ce dispositif est conforme à la norme (s) RSS de la licence-exonéré Industrie Canada. Opération est soumise aux deux conditions suivantes :
1. | Ce dispositif ne peut pas causer de brouillage, et |
2. | Ce dispositif doit accepter toute interférence, y compris le brouillage qui peut causer intempestif de fonctionnement du dispositif. |
Pour assurer la conformité avec les exigences d'Industrie Canada, (limite de Das est de 1,6 W/kg en moyenne pour un gramme de tissu), ces produits ont été évalués et jugés conformes conformément à Industrie Canada, CNR-102 en ce qui concerne le Code de sécurité 6 pour l'exposition humaine aux champs RF.
La valeur SAR la plus élevée signalée en vertu de cette norme lors de la certification du produit lorsqu'il est porté sur le corps :
Nom du produit |
SAR Verdien |
TI-Nspire™ Navigator™ Wireless Cradle |
0.562 W/kg |
TI-Nspire™ Navigator™ Access Point |
0.995 W/kg |
TI-Nspire™ CX Wireless Network Adapter |
0.994 W/kg |
TI-Nspire™ CX Navigator™ Access Point |
0.433 W/Kg |
TI-Nspire™ CX Navigator™ Wireless Network Adapter – v2 |
0.716 W/Kg |
Équipement (ou son antenne de transmission) qui est installé à l'extérieur est soumis à licence et pas pris en charge par les produits énumérés.
On trouvera plus d'informations dans le CNR-102 (http://www.ic.gc.ca/eic/site/smt-gst.nsf/eng/sf01904.html) et dans Code de sécurité 6 notre (http://www.hc-sc.gc.ca/ewh-semt/pubs/radiation/radio_guide-lignes_direct-eng.php).
En vertu de la réglementation d'Industrie Canada, cet émetteur radio risquera uniquement à l'aide d'une antenne de type et de gain maximum (ou moins) pour l'émetteur a été approuvé par Industrie Canada. Pour réduire les interférences radio potentielles à d'autres utilisateurs, le type d'antenne et son gain doivent être choisie que la puissance isotrope rayonnée équivalente (p.i.r.e.) n'est pas plus que celui nécessaire à une communication efficace.
Le dispositif pour la bande 5150-5250 MHz est seulement pour utilisation intérieure réduire le risque de brouillage préjudiciable aux systèmes mobiles par satellite dans la même voie.