Australia Regulatory Compliance
EMC Compliance Statement
In accordance with the provisions on the Radio Regulations of the AS/NZS of Australia, the following radio transmission equipment, after examination, conforms to the provisions:
• | TI-Nspire™ Navigator™ Wireless Cradle |
• | TI-Nspire™ Navigator™ Access Point |
• | TI-Nspire™ CX Wireless Network Adapter |
• | TI-Nspire™ CX Navigator™ Access Point |
• | TI-Nspire™ CX Navigator™ Wireless Network Adapter – v2 |
Operation is subject to the following two conditions: (1) These devices may not cause harmful interference, and (2) these devices must accept any interference received, including interference that may cause undesired operation.
RF Radiation Exposure and Hazard Statement
The products are designed to not exceed the limits for exposure to radio waves recommended by international guidelines, (SAR limit is 2.0 W/kg averaged over 10 grams of tissue). The products listed in the following table have been evaluated under ICNIRP Guidelines for RF exposure from radio frequency devices.
The highest SAR value reported under this standard during product certification when worn on the body:
Product Name |
SAR Value |
TI-Nspire™ Navigator™ Wireless Cradle |
0.242 W/kg |
TI-Nspire™ Navigator™ Access Point |
0.497 W/kg |
TI-Nspire™ CX Wireless Network Adapter |
0.389 W/kg |
TI-Nspire™ CX Navigator™ Access Point |
0.348 W/kg |
TI-Nspire™ CX Navigator™ Wireless Network Adapter – v2 |
0.453 W/kg |
Using higher gain antennas and types of antennas not covered under ICNIRP is not allowed. Installers of the radio and end users of the product must adhere to the installation instructions provided in this manual. This transmitter must not be co-located or operating in conjunction with any other antenna or transmitter.