Working with TI-Nspire™ Applications
Note: For more information, see the appropriate chapter in this guidebook.
To add a TI-Nspire™ application to a problem in a PublishView™ document:
| 1. | Choose one of the following actions to select an application: |
| • | From the TI-Nspire™ Applications pane in the Documents Toolbox, use the mouse pointer to point to the application and drag it to the problem. |
| • | From the menu bar, click Insert and choose an application from the drop-down menu. |
| • | Right-click inside the sheet to open the context menu, click Insert and choose an application from the menu. |
The application is added to the sheet.
| 2. | Using your mouse, grab the handles to resize or position the application object as needed. |
| 3. | Click outside the application frame to accept the dimensions. |
| 4. | To open the menu for the active TI-Nspire™ application, click inside the application. |
The menu opens in the Documents Toolbox above the TI-Nspire™ Applications pane.
Right-click on an application element, such as a cell or function to open the context menu for that item.
| 5. | To work in the application, click an option from the application menu. Click |
Use the TI-Nspire™ Documents pane to open an existing TI-Nspire™ document to add to a PublishView™ document. When you open an existing TI-Nspire™ document, all pages of the document appear in the preview pane. You can move complete problems or individual pages onto the PublishView™ sheet.
Choosing a Working TI-Nspire™ Document
To choose a working document:
| 1. | In the Documents Toolbox, ensure the TI-Nspire™ Documents pane is open. |
| 2. | Click |
The Choose Your Working Document dialog box opens.
| 3. | Navigate to the folder in which the TI-Nspire™ document is stored: |
| • | Click ¤ in the Look in: field to use a file browser to locate a folder. |
| • | From an open folder, click |
| • | Click |
| • | Click |
| • | Click |
| 4. | Select the file, and then click Open. |
The TI-Nspire™ document opens in the TI-Nspire™ Documents pane.
| 5. | To add the TI-Nspire™ document to the PublishView™ document, move one page at a time or one problem at a time to the PublishView™ sheet. |
If you are adding a problem with multiple pages, the pages are stacked on top of each other on the PublishView™ sheet. Move the top page to see the other pages.
Adding an Application to a Problem