Canceling Press-To-Test on Multiple Handhelds
Teachers running TI-Nspire™ CX Premium Teacher Software can cancel Press-to-Test mode remotely on multiple CX and CX II handhelds. The handhelds must be turned on and connected to the teacher's computer by one of these means:
|
•
|
TI-Nspire™ Docking Station or TI-Nspire™ CX Docking Station |
|
•
|
TI-Nspire™ Navigator™ Cradle |
|
•
|
TI-Nspire™ CX Wireless Network Adapter |
|
•
|
A direct connection through a standard USB cable |
Canceling by Using TI-Nspire™ CX Premium Teacher Software
|
1.
|
Make sure the handhelds are turned on and connected to the teacher's computer by one of the means mentioned above. |
|
2.
|
On the Tools menu, select . |
Canceling by Using TI-Nspire™ Student Software
|
1.
|
Connect the handheld to your computer. |
|
2.
|
In the Documents Toolbox, open the Content Explorer. |
|
3.
|
In the Connected Handhelds pane, select the handheld. |
|
4.
|
On the Options menu , select . |
Canceling by Using Send to Class
When a class is in session and students are logged in, you can cancel Press-to-Test by sending the "Exit Test Mode.tns" file to the class. Students not logged in will receive the file when they log in.
|
1.
|
Create an empty .tns file named “Exit Test Mode.tns” and save it in your default TI-Nspire™ folder. |
Note: The file name is case sensitive and must be named as described.
The Select file(s) to send dialog box opens.
|
3.
|
Ensure the tab is open. |
|
4.
|
Navigate to the folder where the "Exit Test Mode.tns" file is located and select it. |
The Select individual(s) dialog box opens.
|
6.
|
Click to send the file to the whole class. To send the file to only those class members who are currently logged in, select the check box. |
Note: To send the file to an individual student, click
, and then click the student name.
|
7.
|
Type Press-to-Test in the field. |
For students who are logged in, the “Exit Test Mode.tns” file is sent, and the connected handhelds exit Press-to-Test mode. The handhelds restart and the operating system loads.
Canceling by Using the Transfer Tool
|
1.
|
Create an empty .tns file named “Exit Test Mode.tns” and save it in your default TI-Nspire™ folder. |
Note: The file name is case sensitive and must be named as described.
|
2.
|
In the Content Workspace, select . |
The Transfer Tool opens.
|
4.
|
Navigate to the folder where the "Exit Test Mode.tns" file is located, and select it to add it to the transfer list. |
|
5.
|
In the Transfer Tool, select the Exit Test Mode.tns file. |
The field becomes active when you select the file name.
|
6.
|
Type Press-to-Test in the field, and click . |
Note: You must type the folder name manually. You cannot select it by navigating to the handheld's Press-to-Test folder.
The “Exit Test Mode.tns” file is sent to the connected handhelds, and Press-to-Test is canceled. The handhelds restart, and the operating system loads.
To cancel Press-to-Test mode on additional handhelds, disconnect the restarted handhelds and connect the other handhelds. The transfer process continues until you stop the transfer.
|
8.
|
To stop the transfer, click . |
|
9.
|
Click when all transfers are complete. |