Removing Columns from Portfolio
There may be times you want to delete files from Portfolio. For example, an incorrect file was sent to or collected from a class. You can remove an assignment from the Assignments pane or from the column header.
1. | Click the assignment name or column header you want to remove. |
2. | Right-click and click Remove From Portfolio. |
The Remove from Portfolio dialog box opens.
3. | Click Remove to delete the file. Click Cancel to cancel the request. |
Note: If a file is saved to the Portfolio Workspace and later deleted from the Class Record, that delete action does not affect the file copy in the Portfolio. The copy remains in the Portfolio Workspace until it is deleted.