Entering Math Expressions in Notes Text
You can include math expressions in Notes text, using the same tools as in other TI-Nspire™ applications.
Math expression boxes have attributes that allow you to control how the expression is displayed.
|
Menu Name |
Menu Option |
Function |
|
|
|
|
|
|
|
When a math box is selected, this option opens a dialog box allowing you to customize the math box. You can hide or show input or output, turn off calculation for the box, insert symbols, change display and angle settings, and allow or disallow the wrapping of expressions and the display of warning indicator after they have been dismissed. You can change the attributes of multiple selected math boxes at the same time. |
|
|
|
Displays a warning indicator after the warning has been dismissed. |
|
|
|
Displays an error after the error has been dismissed. |
Entering an Expression
| 1. | In the Notes work area, position the cursor where you want the expression. |
| 2. | From the Insert menu, select Math Box. —or— Press Ctrl + M (Mac®: Press “+ M). |
An empty math expression box is displayed.
| 3. | Type the expression in the box. You can use the Catalog, if necessary, to insert a function, command, symbol, or expression template. |
| 4. | To exit the math box, click anywhere outside it. |
5: Math Box Options
1: Math Box Attributes