Make sure no other objects are near the access point when it is plugged in.
The access point operating channel or band may affect connectivity.
Important! Always check with your IT administrator before changing access point channels.
| •
|
If the TI-Nspire™ CX Navigator™ access point
is connected, and you are using the TI-Nspire™ CX Wireless Network Adapter – v2 adapters, you can select either a 2.4GHz band or 5GHz band, and you can select a different operating channel. |
| •
|
If you have a mixture of wireless network adapters, you must select the 2.4GHz band. |
The default operating channel for 5GHz in the United States, Canada, and China is 36. The default operating channel for 5GHz in other countries is 149.
To select a different band or operating channel, go to and then click .