Creating Libraries and Library Objects

A document is regarded as a library when it is saved or copied to the designated library folder. The default location is:

• Windows®: My Documents\TI-Nspire\MyLib.
• Mac®: Documents/TI-Nspire/MyLib.
• Handheld: MyLib

If the folder has been inadvertently deleted, you must create it before attempting to use libraries.

You can define library objects using either the Program Editor or the Calculator application. Library objects must be defined with a Define command and must reside in the first problem of a library document.

Note: If you use the Program Editor to define a library function or program, you must store the object and also save the document. Saving the document does not automatically store the object. For more information, see Programming.

Naming restrictions apply to library documents and library objects.

• A library document name must be a valid variable name between 1 and 16 characters long, and it must not contain a period or begin with an underscore.
• A library object name must be a valid variable name between 1 and 15 characters long. It must not contain a period and must not begin with an underscore.