Packaging Lesson Bundles
Packaging lesson bundles creates a "package" folder with a .tilb file. This file contains all files contained in the lesson bundle. You must package the lesson before you can email the lesson bundle (.tilb file) to colleagues or students. By default, the lesson bundle is saved in the following folder:
...\TI-Nspire\New Lesson Bundle1.tilb\package\...
| 1. | Open the Content Explorer. |
| 2. | Navigate to the folder where the lesson bundle is saved. |
| 3. | Select the lesson bundle you want to package. |
| 4. | Right-click to open the context menu, and then click Package Lesson. |
The Lesson Bundle dialog box opens confirming that the .tilb file was created and the lesson bundle was successfully packaged.
| 5. | Click Yes to open the folder where the lesson package is stored. Click No to close the dialog box. |
| 1. | In ComputerContent, navigate to the folder that contains the lesson bundle you want to package. |
| 2. | Click the lesson bundle in the Content pane. The Lesson Bundle details are displayed in the Preview pane. |
| 3. | Use one of the following methods to create the package: |
| • | From the Preview pane, click ¢ in the Files dialog box, and then click Package Lesson Bundle. |
| • | From the Content pane, right-click the lesson bundle name, and then click Lesson Bundles > Package Lesson Bundle. |
The Lesson Bundle dialog box opens confirming that the lesson bundle was created.
| 4. | Click Yes to open the folder where the lesson package is stored. Click No to close the dialog box. |
Packaging a Lesson in the Documents Workspace