Opening a Lesson Bundle

To view and work with files within a lesson bundle, complete one of the following steps to open the lesson bundle file.

▶ Double-click the lesson bundle name.
▶ Select the lesson bundle, and then right-click and click Open.
▶ Select the lesson bundle, click , and then click Open.
▶ Select the lesson bundle, and then press Ctrl + O. (Mac®: “ + O).

When you open a lesson bundle, the files in the bundle are displayed in a separate dialog box.

Note: You cannot open a lesson bundle outside of the TI-Nspire™ software. For example, if you open the folder using the file manager on your computer and double-click the lesson bundle name, it does not automatically launch the TI-Nspire™ software.

Opening Files Within a Lesson Bundle

You can open any file within a lesson bundle on your computer if you have the program associated with the file type.

• When you open a .tns or .tnsp file, the file opens in the Documents Workspace in the TI-Nspire™ software.
• When you open another file type, it launches the application or program associated with that file. For example, if you open a .doc file, it opens in Microsoft® Word.

Use one of the following options to open a file within a lesson bundle:

▶ Double-click the lesson bundle, and then double-click a file within the lesson bundle.
▶ Within a lesson bundle, select the file, and then click ¢ or right-click the file name and select Open.