Creating a New Lesson Bundle
Teachers and students can create new lesson bundles in the Documents Workspace. Teachers can also create new lesson bundles in the Content Workspace.
Complete the following steps to create a new lesson bundle. By default, the new lesson bundle does not contain files.
| 1. | Click |
| 2. | Navigate to the folder where you want to save the lesson bundle file. |
| 3. | Click to open the menu, and then click New Lesson Bundle. |
The new lesson bundle file is created with a default name and placed in your list of files.
| 4. | Type a name for your lesson bundle. |
| 5. | Press Enter to save the file. |
In the Content Workspace, teachers have two options for creating lesson bundles:
| • | When files needed for a lesson bundle are located in different folders, create an empty lesson bundle, and then add files to the lesson bundle. |
| • | If all needed files are located in the same folder, create a lesson bundle with selected files. |
Complete the following steps to create a lesson bundle that does not contain files.
| 1. | Navigate to the folder on your computer where you want to save the lesson bundle. |
Note: If you are using the software for the first time, you may need to create a folder on your computer before creating a lesson bundle.
| 2. | Click |
The new lesson bundle file is created with a default name and placed in the list of files.
| 3. | Type a name for the lesson bundle and press Enter. |
The lesson bundle is saved with the new name and details are shown in the Preview pane.
You can select multiple files within a folder, and then create the lesson bundle. You cannot add a folder to a lesson bundle.
| 1. | Navigate to the folder that contains the files you want to bundle. |
| 2. | Select the files. To select multiple files, select the first file then hold down Shift and click the last file in the list. To select random files, select the first file, and then hold down Ctrl and click the other files to select them. |
| 3. | Click , and then click Lesson Bundles > Create New Lesson Bundle from selected. |
A new lesson bundle is created and placed in the open folder. The lesson bundle contains copies of the selected files.
| 4. | Type a name for the lesson bundle and press Enter. |
The lesson bundle is saved in the open folder and the details are shown in the Preview pane.
Creating a Lesson Bundle in the Documents Workspace
to open the menu, and then click