Using the Lab Cradle
The Lab Cradle can be used in the classroom or remotely. Collect the data with the Lab Cradle, and then retrieve the data later. Store the data on the Lab Cradle until you return to the classroom, and then transfer it to a handheld or computer for analysis.
Using the Lab Cradle with a Handheld
You can connect the Lab Cradle to your handheld to collect or retrieve data.
Using the Lab Cradle with a Computer
The Lab Cradle works with all Windows® and Mac® operating systems currently supported by the TI-Nspire™ Teacher and Student computer software.
Using the Lab Cradle as a Stand-Alone Data Collection Tool
You can use the Lab Cradle in stand-alone mode to collect data either manually or automatically. Press the trigger button to manually start and stop data collection when in stand-alone mode.
Note: For long-term data collections TI recommends you use an AC adapter for a handheld or a remote collection device such as the Lab Cradle.
Before collecting data, set up the data collection parameters using the Vernier DataQuest™ app or use the sensor’s default settings. If you do not change the parameters and use a single sensor, the Lab Cradle collects data using the sensor’s default settings. If you use multiple sensors, the Lab Cradle collects samples beginning with the sensor that has the shortest collection time requirement.
You do not have to reconnect the Lab Cradle to the same computer or handheld to download the data. You can use any computer or handheld running a compatible OS and TI-Nspire™ software to download the data.