Exploring the Lab Cradle

The following graphic shows the front and back of the Lab Cradle.

 

Analog ports. The three BT analog ports used to connect analog sensors. The other side of the cradle has two digital ports for digital sensors.

Battery panel and compartment area. The compartment is where the rechargeable battery is located. Two cross-slotted screws are used to secure the panel to the Lab Cradle.

Digital ports. The two ports used to connect digital sensors.

Reset button. Press to reboot the operating system if the Lab Cradle does not respond to commands. Data may be lost when the Lab Cradle reboots.

Trigger. Lets you begin data collection manually when using the Lab Cradle as a stand-alone data collection tool.

Label. Displays the serial number and other hardware information.

Handheld transfer connector. Connects the handheld to the Lab Cradle for collecting or transferring data.

Locking latch. Locks the Lab Cradle and handheld together.