Charging the Lab Cradle
You can charge the Lab Cradle in a number of ways.
• | Wall charger |
• | USB Cable connected to a computer |
• | TI-Nspire™ Navigator™ Cradle Charging Bay |
Charging with an AC Wall Charger
Connect the plug to a standard AC wall outlet and the mini-B USB connector to the TI-Nspire™ Lab Cradle.
Charging with a USB Cable
The Lab Cradle can be charged using a standard USB cable. Attach the mini-B connector to the Lab Cradle and the USB type A connector into the computer.
The Lab Cradle will fully charge in less than 12 hours.
Charging with a Charging Bay
Use the TI-Nspire™ Navigator™ Cradle Charging Bay to charge five Lab Cradles at the same time. A full charging bay with dead Lab Cradle units fully charges those units in less than 12 hours.
You can leave the Lab Cradle in the charging bay even if fully charged. You can recharge at any time regardless of the current charge level.
The charging bay is only included in certain bundled packages. The charging bay works with Lab Cradles or with Lab Cradles connected to handhelds.